Expressions.Numeric value function
            A function returning a numeric value
Format
Remarks
A numeric function returns a numeric value and can be any one of the following:
- An EXTRACT function to return a date or time field from a datetime or interval. Refer to Extract expression for more details.
 - A function returning the length of an item, such as CHAR_LENGTH, BIT_LENGTH, or OCTET_LENGTH. Refer to Length expression for more details.
 - A POSITION function to return the position of a substring within another string. Refer to Position expression for more details.
 - An ABS function to return the absolute value of an expression. Refer to Absolute value expression for more details.
 - A MOD function to return the modulos of a value. Refer to Modulus expression for more details.
 - A LN function to return the natrual logarithm of a value. Refer to Natural logarithm for more details.
 - A EXP function to return e raised to the power of a value. Refer to Exponential function for more details.
 - A POWER function to return one value raised to the power of another. Refer to Power function for more details.
 - A SQRT function to return square root of another. Refer to Square root for more details.
 - A FLOOR function to return a rounded down value of another. Refer to Floor function for more details.
 - A CEILING function to return a rounded up value of another. Refer to Ceiling function for more details.
 - An OCCURRENCES_REGEX function to return the number of times a pattern exists in another string. Refer to Regex occurrences function for more details.